SCDU037 May 2024 TMUXHS4612
Most interfaces require AC coupling between the transmitter and receiver. For example, the DisplayPort specification requires AC coupling capacitors in the range of 75 – 200nF on the TX. By default, the TMUXHS4612-EVM is populated with 0Ω resistors on the input and output which can be replaced with capacitors if needed.