SCEU031B August   2024  – October 2024 TPLD801

PRODUCTION DATA  

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Functional Blocks
      1. 2.1.1 Test Points
      2. 2.1.2 Programmer Header Block (P1)
      3. 2.1.3 External Connection Header Block
      4. 2.1.4 GPI Protection Block
      5. 2.1.5 DRL Socket
      6. 2.1.6 SW or LED Testing Blocks
      7. 2.1.7 GPI Switch Testing Block
  9. 3Software
    1. 3.1 Using the TPLD801-DRL-EVM
      1. 3.1.1 Equipment Needed for Programming
      2. 3.1.2 Installing Software
    2. 3.2 Configuring a TPLD Device
      1. 3.2.1 TPLD801-DRL-EVM Setup for Programming
      2. 3.2.2 Inserting a TPLD801DRL into the DRL Socket
      3. 3.2.3 Connecting the TPLD801-DRL-EVM to a TPLD-PROGRAM Board
      4. 3.2.4 Temporarily Configuring a TPLD Device
      5. 3.2.5 Permanently Programming a TPLD Device
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layout
      1. 4.2.1 PCB Overview
    3. 4.3 Bill of Materials
  11. 5Additional Information
    1. 5.1 Trademarks
  12. 6Revision History

Permanently Programming a TPLD Device

This section covers using InterConnect Studio to permanently program a TPLD801. Permanently programmed devices retain the configuration the devices are programmed with after power is reset.

Permanently programmed devices must not be permanently programmed again to avoid damaging the device.

  1. Open the desired configuration to be permanently programmed in the TPLD801 in InterConnect Studio.
  2. Open the Configure Settings by selecting the three dots icon beside the CONFIGURE TPLD801 button.
  3. Select Permanently Configure Device. If using a TPLD-PROGRAM to power the EVM, then leave the Power Source as Programmer. Select OK.
    TPLD801-DRL-EVM Permanent Programming
                            in ICS Figure 3-7 Permanent Programming in ICS
  4. Select the serial port connected to the TPLD-PROGRAM, then select OK again.
    1. Some LEDs on the TPLD801-DRL-EVM can flash during the programming sequence, which is normal.
    2. If the programming fails, check the connections between the EVM and the computer, make sure SW8 is ON, check the connection between the TPLD device and the socket contacts, confirm that the shunt setup is correct according to Section 3.2.1 and retry.
  5. Remove power from the EVM before removing the permanently programmed TPLD801.