All cables included are keyed and can
only be plugged in when facing the correct direction. If a cable cannot be inserted
with the application of a gentle amount of force, try swapping the orientation of
the cable and making sure that the header housings are unobstructed before trying
again. Forcing the connections can cause damage to the cables and boards.
- Connect the programmer board
to a computer running InterConnect Studio using the provided USB cable. Make
sure that a good connection is made between the TPLD-PROGRAM and the
computer, indicated by the two blue LEDs on the TPLD-PROGRAM both being on.
An example of a fully connected EVM can be seen in Section 3.1.
- Connect the TPLD-PROGRAM to
the TPLD801-DRL-EVM using the provided 14-position ribbon cable. Make sure
that a good connection is made between the TPLD801-DRL-EVM and the
TPLD-PROGRAM, indicated by the 3V3 LED in the top left of the EVM being
on.