SFFS222 October 2023 TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
This section provides a brief summary of the diagnostic mechanisms available on the TMS320F280015x MCU device family. The diagnostic mechanisms are arranged as per the device portioning given in Figure 5-1. At places where the safety mechanism is applicable for more than one component, it is placed at an appropriate place based on the applicable use case scenario. For a detailed description or implementation details for a diagnostic, see the device-specific technical reference manual.