SFFS298 December   2021 AMC1300B-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the AMC1300B-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the AMC1300B-Q1 pin diagram. For a detailed description of the device pins see the Pin Configuration and Functions section in the AMC1300B-Q1 data sheet.

GUID-20201121-CA0I-VQCN-1MML-H1VCNS1X7KRD-low.gif Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • Differential RC filter between INP and INN.
    The series resistors are sized to limit the input currents into INP and INN to <10 mA in all circumstances (for example, if the device is unpowered and the input signal is applied).
  • INN is connected to GND1 through the filter resistor.
  • For pins on high side:
    Short-circuited to ground means short to GND1.
    Short-circuited to supply means short to VDD1.
  • For pins on low side:
    Short-circuited to ground means short to GND2.
    Short-circuited to supply means short to VDD2.

Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VDD11Device high side unpowered. Fail-safe output (see data sheet for more details).B
INP2INP stuck low (GND1). Differential output (VOUTP – VOUTN) = –VINN x 8.2 with common-mode voltage approximately 1.44 V.B
INN3INN stuck low (GND1). Differential output (VOUTP – VOUTN) = VINP x 8.2 with common-mode voltage approximately 1.44 V.D
GND14No effect. Normal operation.D
GND25No effect. Normal operation.D
OUTN6OUTN stuck low (GND2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time.A
OUTP7OUTP stuck low (GND2). Excess current consumption from VDD2. Device damage plausible if condition is present for extended period of time.A
VDD28Device low side unpowered. OUTP and OUTN pins are driven to GND2.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VDD11Device high side unpowered. Fail-safe output (see data sheet for more details).B
INP2Differential output (VOUTP – VOUTN) undetermined, but with tendency to output +FS.B
INN3Differential output (VOUTP – VOUTN) undetermined.B
GND14Device high side unpowered. Fail-safe output (see data sheet for more details).B
GND25Device behavior undetermined. VOUTN and VOUTP undetermined.B
OUTN6Differential output (VOUTP – VOUTN) undetermined.B
OUTP7Differential output (VOUTP – VOUTN) undetermined.B
VDD28Device low side unpowered. VOUTN and VOUTP undetermined.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
VDD11INPINP stuck high (VDD1). In case VCM < VCMov, differential output (VOUTP – VOUTN) = +FS. In case VCM ≥ VCMov, fail-safe output (see data sheet for more details).B
INP2INNDifferential input shorted. Differential output (VOUTP – VOUTN) = 0 VB
INN3GND1INN stuck low (GND1). Differential output (VOUTP – VOUTN) = VINP × 8.2 with common-mode voltage approximately 1.44 V.D
GND14GND2Not considered. Corner pin.D
GND25OUTNOUTN stuck low (GND2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time.A
OUTN6OUTPDifferential output (VOUTP – VOUTN) = 0 V with common-mode voltage approximately 1.44 V. Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time.A
OUTP7VDD2OUTP stuck high (VDD2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time.A
VDD28VDD1Not considered. Corner pin.D
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VDD11No effect. Normal operation.D
INP2INP stuck high (VDD1). In case VCM < VCMov, differential output (VOUTP – VOUTN) = +FS. In case VCM ≥ VCMov, fail-safe output (see data sheet for more details).B
INN3INN stuck high (VDD1). In case VCM < VCMov, differential output (VOUTP – VOUTN) incorrect. In case VCM ≥ VCMov, fail-safe output (see data sheet for more details).B
GND14Device high side unpowered. Fail-safe output (see data sheet for more details).B
GND25Device low side unpowered. OUTP and OUTN pins are driven to GND2.B
OUTN6OUTN stuck high (VDD2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time.A
OUTP7OUTP stuck high (VDD2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time.A
VDD28No effect. Normal operation.D