SFFS347 December   2021 LM25149

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the LM25149. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to Ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the LM25149 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the LM25149 data sheet.

Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
AVSS1AVSS is ground. VOUT = expected VOUTD
INJ2Active EMI filtering will not work but the regulator will continue regulating. VOUT = expected VOUTC
CNFG3Active EMI filtering will be disabled. VOUT is unaffected.C
RT4VOUT will attempt to regulate at maximum fSW, causing maximum power dissipation.B
EXTCOMP5VOUT = 0 VB
FB6Internal FB mode, VOUT = expected VOUTD
External FB mode, VOUT = VINA
AGND7AGND is GND. VOUT = expected VOUTD
VDDA8VOUT = 0 V, no switching, loaded VCC outputB
VCC9VOUT = 0 V, no switching, loaded VCC outputB
PGND10PGND is GND. VOUT = expected VOUTD
LO11VOUT = 0 V, VCC regulator loaded to the current limitB
VIN12VOUT = 0 VB
HO13VOUT = 0 V, VCC regulator loaded to the current limitB
SW14VOUT = 0 V. High-side FET is shorted from VIN to GND.A
CBOOT15VOUT = 0, VCC regulator loaded to the current limitB
VCCX16VOUT = expected VOUT. The internal VCC regulator provides bias voltage.C
PG17If in single phase, PG has no effect on operation. VOUT = expected VOUT C
If in interleaved primary mode, the secondary will detect no clock input and will shut down. Secondary phase is disabled and primary phase can current limit.B
PFM/SYNC18VOUT = expected VOUT. No synchronization will be available and the LM25149 will be in FPWM mode.C
EN19VOUT = 0 V. The LM25149 enters shutdown.C
ISNS+20VOUT = 0 V; HO damagedA
VOUT21VOUT = 0 V. Current limit reached and hiccup mode occurs.B
AEFVDDA22AEFVDDA = VCC. VCC is shorted and VOUT = 0 V. VCC is loaded.B
SEN23Active EMI filtering will not work but the regulator will continue regulating. VOUT = expected VOUTB
REFAGND24REFAGND is ground. VOUT = expected VOUTD
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
AVSS1Active EMI filtering will not work but the regulator will continue regulating. VOUT = expected VOUTC
INJ2Active EMI filtering will not work but the regulator will continue regulating. VOUT = expected VOUTC
CNFG3VOUT will continue operating normally. CNFG is used during start-up and enables AEF.C
RT4RT will regulate to 500 mV, but the internal oscillator will not function.B
EXTCOMP5VOUT will oscillate. If VOUT oscillates to VIN, damage can occur if VIN > 60 V.A
FB6Internal FB mode, VOUT = expected VOUTD
External FB mode, VOUT = VINA
AGND7VOUT is indeterminate.B
VDDA8Poor noise immunityC
VCC9VOUT = 0 VB
PGND10VOUT = 0 VB
LO11VOUT = expected VOUT with reduced efficiencyC
VIN12VOUT = 0 VC
HO13If HO is opened while HO to SW has voltage, the high-side FET will never turn off. VOUT = VINA
SW14VOUT is indeterminate. The CBOOT floating rail has no reference to the actual SW node. VOUT = VINA
CBOOT15VOUT = 0 VB
VCCX16VCCX is held to ground by a weak pulldown. VOUT = expected VOUTD
PG17If in single phase, PG has no effect on operation. VOUT = expected VOUTC
If in interleaved primary mode, the secondary will detect no clock input and will shut down. The secondary phase is disabled and primary phase can current limit.B
PFM/SYNC18VOUT = expected VOUTD
EN19VOUT = expected VOUTD
ISNS+20The OPEN ISNS+ pin will block current limit and cause VOUT oscillations.A
VOUT21VOUT = 0 VB
AEFVDDA22Active EMI filtering will not function.C
SEN23Active EMI filtering will not function.C
REFAGND24Active EMI filtering will not function.C
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
AVSS1INJActive EMI filtering will not function. VOUT = expected VOUTC
INJ2CNFGActive EMI filtering will not function. VOUT = expected VOUTC
CNFG3RTVOUT = expected VOUT with erratic switchingB
RT4EXTCOMPCOMP cannot regulate down due to clamping by the internal RT.B
EXTCOMP5FBExternal FB mode: COMP will regulate to .8 V and the output will be unregulated. VOUT = any voltageB
Internal FB mode: COMP will rise up to VDD. VOUT = VINA
FB6AGNDExternal FB mode: VOUT = VINA
Internal FB mode: VOUT = expected VOUTD
AGND7VDDAVDDA will be grounded. VOUT = 0 VB
VDDA8VCCVOUT = expected VOUTD
VCC9PGNDVCC will be grounded. VOUT = 0 VB
PGND10LOVOUT = 0 V. VCC is loaded by LO driver.B
LO11VINVOUT = 0 V. The driver will be damaged if VIN > 6.5 V.A
VIN12HOVOUT = VINA
HO13SWVOUT = 0 VB
SW14CBOOTVOUT = 0 VB
CBOOT15VCCXVOUT < 5 VA
VCCX16PGPG pulldown can damage. VOUT = expected VOUTA
PG17PFM/SYNCVOUT = expected VOUTC
PFM/SYNC18ENVOUT = expected VOUTA
EN19ISNS+EN is high voltage rated. VOUT = expected VOUT if VOUT > 1 V. If VOUT < 1 V, the device is disabled.B
ISNS+20VOUTCurrent limit is disabled since the current limit resistor would be shorted. VOUT cannot regulate since current mode feedback is shorted.A
VOUT21AEFVDDAActive EMI filtering will not function and damage will occur if VOUT > 6.5 V. VOUT = expected VOUTA
AEFVDDA22SENActive EMI filtering will not function. VOUT = expected VOUTC
SEN23REFAGNDActive EMI filtering will not function. VOUT = expected VOUTC
REFAGND24AVSSNo impactD
Table 4-5 Pin FMA for Device Pins Short-Circuited to VIN
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
AVSS1Active EMI filtering will not function, high VIN currentA
INJ2Active EMI filtering will not function, high VIN currentA
CNFG3VOUT = VINA
RT4VOUT = 0 V; high VIN currentA
EXTCOMP5This will bring VDDA up to VIN. VOUT = VIN.A
FB6This will bring VDDA up to VIN. VOUT = VINA
AGND7VOUT = VIN; high VIN currentA
VDDA8If VIN < 6.5 V, VOUT = expected VOUTD
If VIN > 6.5 V, exceeds maximum ratings and VDDA is damaged.A
VCC9If VIN < 6.5 V, VOUT = expected VOUTD
If VIN > 6.5 V, exceeds maximum ratings and VCC is damaged.A
PGND10VOUT = VIN; high VIN currentA
LO11For VIN < 6.5 V, VOUT = 0; excess current from VINB
For VIN > 6.5 V, exceeds maximum ratings and pin LO is damaged.A
VIN12N/AD
HO13For VIN < 6.5 V, VOUT = dropout lower than VIN, no switching, excess current from VINB
For VIN > 6.5 V, exceeds maximum ratings and HO is damaged, VOUT = VINA
SW14VOUT = VIN, excess current from VIN. LO turns on and shorts against VIN.A
CBOOT15For VIN < 6.5 V, VOUT = expected VOUT, erratic switchingB
For VIN > 6.5 V, exceeds maximum ratings and the CBOOT pin is damaged, HO damaged. VOUT = VINA
VCCX16If VCCX = VOUT, for VIN < 6.5 V, VOUT = VINB
For VIN > 6.5 V, exceeds maximum ratings and VCCX is damaged.A
PG17For VIN < 6.5 V, VOUT = expected VOUT, PG forced highB
For VIN > 6.5 V, exceeds maximum ratings and PG is destroyed.A
PFM/SYNC18If PFM = GND, VOUT = 0 V, excess current from VINB
If PFM = VDDA and VIN < 6.5 V, VOUT = expected VOUT and erratic switching.B
If VIN > 6.5 V, exceeds maximum ratings and PFM is damaged. VOUT = expected VOUTA
EN19The part will be always on. VOUT = expected VOUTC
ISNS+20If VIN < 60 V, VOUT = VINB
If VIN > 60 V, exceeds maximum ratings and CS is damaged.A
VOUT21If VIN < 60 V, VOUT = VINB
If VIN > 60 V, exceeds maximum ratings and CS is damaged.A
AEFVDDA22Active EMI filtering will not function, high VIN currentA
SEN23Active EMI filtering will not function, high VIN currentA
REFAGND24Active EMI filtering will not function, high VIN currentA