SFFS700 May 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Clock setup for the TMS320F28P65xD/S MCU device family includes selecting the appropriate clock source, configuring the PLL multiplier, waiting for the lock status and switching the clock to the PLL output once the internal lock status is set. The time required for the PLL lock sequence can be profiled using on-chip timer to detect faults in the PLL wrapper logic. Once the PLL is locked, the frequency of the output clock can be checked by using the following: