SFFS897 May 2024 SN4599-Q1
This section provides a Failure Mode Analysis (FMA) for the pins of the SN4599-Q1 (SOT-23 package). The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the pin diagram. For a detailed description of the device pins, please refer to the Pin Configuration and Functions section in the SN4599-Q1 data sheet.
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
SEL | 1 | SEL stuck low. Cannot control switch states | B |
VDD | 2 | Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
GND | 3 | No effect, normal operation | D |
S1 | 4 | Corruption of signal passed onto the D pin. If there is no limiting resistor in the switch path device damage possible Device unpowered. | A |
D | 5 | Corruption of signal passed onto the S1/S2 pins. If there is no limiting resistor in the switch path device damage possible | A |
S2 | 6 | Corruption of signal passed onto the D pin. If there is no limiting resistor in the switch path device damage possible | A |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
SEL | 1 | Loss of control of SEL pin. Cannot control switch. | B |
VDD | 2 | Device unpowered. Device not functional. | B |
GND | 3 | Device unpowered. Device not functional. | B |
S1 | 4 | Corruption of signal passed onto the D pin. | B |
D | 5 | Corruption of signal passed onto the S1/S2 pins. | B |
S2 | 6 | Corruption of signal passed onto the D pin. | B |
Pin Name | Pin No. | Shorted To | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
SEL | 1 | VDD | SEL stuck high. Can no longer switch signal path of the device | B |
VDD | 2 | GND | Device is unpowered. Device is not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage may be plausible. | A |
GND | 3 | S2 | Not considered. This is a corner pin. | D |
S2 | 4 | D | Corruption of signal passed onto the D pin. | B |
D | 5 | S1 | Corruption of signal passed onto the S1/S2 and D pins. | A |
S1 | 6 | VDD | Not considered. This is a corner pin. | D |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
SEL | 1 | SEL stuck high. Cannot control switch states | B |
VDD | 2 | No effect; normal operation | D |
GND | 3 | Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met. Otherwise, device damage may be plausible. | A |
S2 | 4 | Corruption of signal passed onto the D pin. If there is no limiting resistor in the switch path device damage is possible. | A |
D | 5 | Corruption of signal passed onto the S1/S2 pins. If there is no limiting resistor in the switch path device damage is possible. | A |
S1 | 6 | Corruption of signal passed onto the D pin. If there is no limiting resistor in the switch path device damage is possible. | A |