SLAA558A November 2012 – October 2018 MSP430F5212 , MSP430F5214 , MSP430F5217 , MSP430F5219 , MSP430F5222 , MSP430F5224 , MSP430F5229 , MSP430F5252 , MSP430F5253 , MSP430F5254 , MSP430F5255 , MSP430F5256 , MSP430F5257 , MSP430F5258 , MSP430F5259
The DVIO supplied general-purpose I/Os are multiplexed with other digital functions in the device, and these digital functions’ I/O circuits are also powered from DVIO. On the F522x and F521x devices, some of the secondary digital functions that are shared with the DVIO supplied I/Os include timer capture compare functions, serial communication functions (USCI UART, SPI, or I2C), comparator output, SMCLK output, and MCLK output. See the signal descriptions table in MSP430F522x, MSP430F521x Mixed-Signal Microcontrollers for details.
On the F522x and F521x devices, Port 4 supports port mapping and resides on the DVIO supply domain. Any of the secondary digital functions specified in the port mapping table can be mapped to Port4, and their respective I/O circuitry is supplied by DVIO. See the port mapping table in the Peripherals section of the data sheet for details.
NOTE
In split supply I/O systems, if external pullup resistors are connected to any of the DVIO supplied pins (for example, the USCI I2C pins – SDA and SCL), tie the external pullups to the DVIO supply and not to DVCC.
Other DVIO supplied digital pins on the F522x and F521x devices include: