SLAA870 February 2019 AFE7422 , AFE7444
As for the transmitter, each DAC in the AFE74xx contains a dual-band digital upconverter (DUC), also known as a multi-DUC, and each DUC contains two, independently programmed, back stage NCO accumulators. Figure 4 shows the basic block diagram of one TX_TOP (including two transmitters) in the AFE74xx, where the signal processing features of each of the two multi-DUCs is highlighted in the shadowed area.