SLAA871 January 2019 AFE7422 , AFE7444
The AFE74xx support the internal loopback of the 20-bit digital stream from the receiver to the transmitter with the SerDes bypassed. This feature can be used in applications such as repeaters, where the digital output of the RX must be fed back to the input of TX. With this loopback feature, users do not have to physically connect the STX lanes to SRX lanes on their board (through FPGA or ASIC), and gives the following advantages: