All trademarks are the property of their respective owners.
This section discusses the physics of sound waves and the benefits of using ultrasonic sensors in a variety of applications.
Ultrasonic sensors can measure distance and detect the presence of an object without making physical contact. They do so by producing and monitoring an ultrasonic echo. Depending on the sensor and object properties, the effective range in air is between a few centimeters up to several meters. The ultrasonic sensor (or transducer) generates and emits ultrasonic pulses that are reflected back towards the sensor by an object that is within the field of view of the sensor.
The ultrasonic sensor is a piezoelectric transducer, which is able to convert an electrical signal into mechanical vibrations, and mechanical vibrations into an electrical signal. Therefore, in a monostatic approach, the ultrasonic sensor is a transceiver which operates as both a speaker and microphone at a single frequency.
The sensor is able to capture the difference in time between the emitted and received echo. Because the speed of sound is a known variable, the captured round-trip time can be used to calculate the distance between the sensor and object. Equation 1 shows the Ultrasonic Distance Calculation.
This method of ultrasonic sensing is a time-of-flight measurement based on the propagation time of sound. Note that the velocity of sound through air varies by temperature. In dry air at 20°C (68°F), the speed of sound is 343 m/s, or a kilometer in 2.91 s. For more information on the relationship between the velocity of sound and temperature, see Section 3.4.
Ultrasonic sensors can detect a variety of materials, regardless of shape, transparency, or color. The only requirement for ultrasonic sensing is that the target material is a solid or liquid. This enables contactless detection of:
These materials are able to reflect sound back towards the sensor through the air. Certain objects can be more difficult to detect, like angled surfaces that direct the echo away from the sensor, or permeable targets like sponge, foam, and soft clothing. These absorb more reflected ultrasonic energy.