SLAA907D September 2019 – December 2021 PGA450-Q1 , PGA460 , PGA460-Q1 , TDC1000 , TDC1000-Q1 , TDC1011 , TDC1011-Q1 , TUSS4440 , TUSS4470
Ultrasonic transducers operate at frequencies in the range of 30–500 kHz for air-coupled applications. As the ultrasonic frequency increases, the rate of attenuation increases. Thus, low-frequency sensors (30–80 kHz) are more effective for long range, while high-frequency sensors are more effective for short range. Higher frequency sensors (80–500 kHz) also reduce the ringing-decay, which allows for a shorter minimum detection range. For liquid level sensing, transducers in the 1-MHz range are often used. For more information on liquid level sensing using ultrasonic technology, read Ultrasonic Sensing Basics for Liquid Level Sensing application report (SNAA220).
The relationship between frequency, resolution, directivity, attenuation, and distance can be observed with the following relation:
↑ Frequency :: ↑ Resolution :: ↑ Narrower Directivity :: ↑ Attenuation :: ↓ Distance
Transducers can have narrow (15°) to wide field of views (180°). The higher the frequency, the narrower the field of view. A narrow field of view using a low-frequency transducer can also be achieved by adding a "horn" around the transducer to direct its echoes into a more narrow pattern.