SLAAE64 may 2023 AFE58JD48 , DAC81001 , DAC8801 , DAC8830 , OPA2210 , REF5010 , REF5040 , THS4130
Ultrasound imaging is based on the pulse-echo method, by sending ultrasound waves to the objects being imaged and receiving echo signals. It is also known that the emitted ultrasound wave amplitude gets smaller as the wave penetrates tissue, a phenomenon called attenuation. Signals that are reflected immediately after transmission are very strong because the signals are from reflections close to the surface; reflections that occur long after the transmit pulse are very weak because these signals are reflecting from deep in the body. If the ultrasound image was formed directly by the raw returned echoes, the image appears lighter in the superficial layers and darker in deep layers. A way to overcome ultrasound attenuation is time gain control or compensation (TGC), in which signal gain is increased as time passes from the emitted wave pulse. This correction makes equally echogenic tissues look the same even if the tissue is located in different depths. TI’s low-noise analog front ends (AFEs) have a TGC feature that supports ultrasound applications because the AFEs can alter the gain of the receiver as a function of time. The ultrasound signal incident on the receiver decreases in amplitude as a function of the time elapsed since transmission, and the TGC helps achieve the best possible signal-to-noise ratio (SNR), even with the decreasing signal amplitude.
This application note describes the specifications and design considerations of three proposal circuits used for generating a time-varying control voltage to drive multiple AFE receiver chips. Figure 1-1 shows the signal chain of the AFE58JD48 analog front end. The TGC function is integrated and is implemented using an attenuator that can be controlled with a control voltage, VCNTL. External circuitry comprised of a digital-to-analog converter (DAC) and operational amplifier (op amp) generates the control signal. The input signal for the DAC is a time-varying digital control from a field programmable gate array (FPGA) that can also handle the beamforming operation required in an ultrasound application.
VCNTL attributes from the point of view of the AFE are provided in the following list.