SLAAE71 December 2022 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
Conditional code execution
One commonly used software structure is to use a conditional wake-up and code execution structure. A common wake-up source is RTC. If the MCU does not have RTC, the application can use TIMG as a replacement. Find the static current information in the data sheet.
Non-blocking programming
In low-power applications, it is necessary to avoid blocking mode by using while loop. Using non-blocking mode paired with interrupts and polling to wake up the CPU to process tasks is more acceptable. Although it will sacrifice time and resources to wake up and respond to interrupt sources, push and pop the stack, it can save more power.
Optimize code size
Small code size means that CPU needs less time to finish tasks in active mode. The easiest way is to choose a highly optimized compiler such as TI Arm Clang Compiler and leverage the supplied code optimization levels. You can also spend some time or coding skills to realize this aim.