SLAAE76B march 2023 – june 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
The MSPM0G OPA is a zero-drift chopper stabilized operational amplifier with a programmable gain stage. The OPA can used for signal amplification and buffering and can work in general-purpose mode, buffer mode and PGA mode.
When using the OPA in general-purpose mode, add an external resistor and capacitor to create the amplifier circuit. But when using buffer mode, it can be configured through software. For PGA mode, software can configure up to 32x PGA gain.
When two or more OPAs are available on a device, the two can be combined to form a differential amplifier. The output equation for the differential amplifier is given by the Vdiff equation in Figure 6-2.
Alternately, when two or more OPAs are available on a device, they can be combined to form a multi-stage or cascaded amplifier. Using the programmable input muxes, all combinations of inverting and non-inverting multi-stage amplifiers can be implemented. The output equation for the noninverting to noninverting cascaded amplifier is given by the Vout equation in Figure 6-3.