SLAAE76B march 2023 – june 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
The VBOOST circuit in the PMU generates an internal VBOOST supply that is used by the analog muxes in COMP, GPAMP, and OPA, if present on a device. The VBOOST circuit enables consistent analog mux performance across the external supply voltage (VDD) range.
SYSCTL automatically manages the enable request for the VBOOST circuit based on the following parameters:
VBOOST is disabled by default following a SYSRST. It is not necessary for application software to enable the VBOOST circuit before using the COMP, OPA, or GPAMP. When a COMP, OPA, or the GPAMP is enabled by application software, SYSCTL also enables the VBOOST circuit to support the analog peripheral.
The PMU provides a temperature and supply voltage stable bandgap voltage reference, which is used by the device for internal functions including:
The bandgap reference is enabled in RUN, SLEEP, STOP modes. It operates in a sampled mode in STANDBY to reduce power consumption. It is disabled in SHUTDOWN mode. SYSCTL manages the bandgap state automatically so that no user configuration is required.