Confirm the items below before
starting LFU firmware upgrade process:
- Make sure bootloader firmware
already programmed into device via SWD interface.
- Build application project and
generate the .txt file needed for firmware upgrade. Suggest generating both
application code 1 and application code 2 for evaluation purpose.
- Prepare .txt format BSL password
file.
Now you can launch PC GUI tool by
double-click the file MSPM0_LFU_BSL_GUI.exe at the folder “…\MSPM0 LFU Bootloader
Implementation v1.1\BSL_GUI_EXE”. The following steps describe how to perform
firmware upgrade process:
- Check application code status,
which application code is executed or no application code in the device.
- Select application code for
firmware upgrade evaluation.
- If no application code in
the device, you can select either application code 1 or application code
2 for firmware upgrade.
- If application code 1 is
executed in the device, select application code 2 for firmware
upgrade.
- If application code 2 is
executed in the device, select application code 1 for firmware
upgrade.
- Choose a password file based on
the format of the default one in the input folder.
- Click the download button to do
the firmware update.