SLAAED9 November 2023 TAA5412-Q1 , TAC5311-Q1 , TAC5312-Q1 , TAC5411-Q1 , TAC5412-Q1
Figure 5-1 shows the suggested flow for setting up fault diagnostics. Each feature is described in more detail in the following sections. Some applications do not use all features or rely on the default values in the configuration registers. At a minimum, the user must power up MICBIAS and enable the channel diagnostics.