Figure 8-2 shows a section of the Advanced Mode Tab that allows the user to adjust
the monitored input faults with a programmable threshold from 0 to 450 mV. The
single point sliders are set to the default threshold for each fault at
initialization.
- The Threshold Range Scale
check box allows the user to scale all of the configuration thresholds by two
times.
- The INxM pins of Single Ended
Configuration check box excludes the INxM pins from being scanned for
diagnostics.
- The AC Coupled channel
pins check box configures the device to include the AC coupled channels
in the scan for diagnostics. Enabling this box coincides with using one channel
for DC diagnostics while the other channel has an AC-coupled MIC input as shown
in Figure 2-3.