SLAAED9 November 2023 TAA5412-Q1 , TAC5311-Q1 , TAC5312-Q1 , TAC5411-Q1 , TAC5412-Q1
This fault is triggered if the difference between the voltage measured at the input pin and the voltage measured at the MICBIAS pin is greater than 0 V and less than the programmed threshold. This fault is programmable from 0 V to 450 mV with a programming step size of 30 mV. This fault uses the actual voltage measured at the MICBIAS pin, which can differ slightly from the programmed MICBIAS value.