Here is the current detection block
diagram. We can see that this solution utilizes:
- Two high precision internal OPAs.
One OPA used as a buffer for DAC. Another used to generate gain for the voltage
across the shunter resistor.
- One internal DAC. Used to
generate dynamic bias voltage for current detection paired with OPA0.
- Flexible internal gain, which is
the key point to realize different detection range. If you increase the gain,
then the detection range will be smaller, but its resolution will be increased
as well.
- Internal SAR ADC. Used to
calibrate and detect the voltage output from OPA0.