SLAAEF1A August   2023  – July 2024 AFE11612-SEP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Laser and Semiconductor Optical Amplifier Biasing
  6. 3EML Negative Bias Voltage
  7. 4Photodiode Detection Measurement
  8. 5Variable Optical Attenuator Control
  9. 6Summary
  10. 7References
  11. 8Revision History

Laser and Semiconductor Optical Amplifier Biasing

Laser diodes and semiconductor optical amplifiers (SOAs) require a precision current source and current monitoring to be accurately biased. The AFE11612-SEP has twelve 12-bit DACs that can be configured to be a precision current source with external circuitry. The circuit in Figure 2-1 uses the AFE11612-SEP DAC outputs, external operational amplifiers (op amps), and external MOSFETs to supply a programmable current to a ground-referenced load.

 Laser Diode Bias CircuitFigure 2-1 Laser Diode Bias Circuit

The first op amp stage uses RSET and the DAC output voltage (VDAC) to set the reference current. VDAC is applied to the noninverting input of OPA1, which sets the high-side of RSET to the same voltage. This reference current (ISET) is calculated with Equation 1.

Equation 1. ISET=VDACRSET

The second op amp stage is a current-mirror with a gain set by RA and RB. The current flowing through RA is equal to ISET. This creates a voltage drop across RA. RB has the same voltage drop due to the op amp OPA2 feedback forcing the voltage at the low-side of RB. Thus, with RA and RB having the same voltage drop, the current flowing through RB can be tuned by picking specific resistor values. This current (IMIR) is the current that is used by the load. Use Equation 2 and Equation 3 to calculate the current gain.

Equation 2. ISET×RA=IMIR×RB
Equation 3. Current Gain=ISETIMIR=RARB

The total gain of the system can be calculated by Equation 4.

Equation 4. IMIR=VDAC×RARSET×RB

For additional information on using voltage DACs to create programmable current sources, see 8-Channel, 16-Bit, 200-mA Current Output, Digital-to-Analog Converter Reference Design and Programmable, Two-Stage, High-Side Current Source Current.

Additionally, the AFE11612-SEP features an ADC with differential inputs which can assist in measuring the voltage differential across RB to monitor current. The AFE11612-SEP ADC has a range of 5 V, so the PVDD voltage must be taken into account when using the ADC for measurements. For use in higher voltage applications, an INA or a voltage divider circuit can be used to measure the voltage across RB.

The AFE11612-SEP also has two remote temperature monitors that trigger an alarm when they detect temperature that exceeds a user-determined value. These can be placed near temperature sensitive components to make sure that the host is informed when the devices are overheating.