SLAAEF6 September 2023 MSPM0L1105 , MSPM0L1106 , MSPM0L1306 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
Software is a powerful piece of the MSPM0 PIR Motion Detector. As mentioned, the software controls the analog signal chain and feedback loops. The signal is also being sampled via the ADC, which allows digital filter techniques to be applied to the detection and feedback loops. This application note includes source code for the PIR motion detection demo. This demo software is intended to accelerate the development of a PIR solution using MSPM0L1306 MCU, but this software is only a part of a complete system and is intended to be used only as a reference.