SLAAEF9 November 2023 MSPM0L1306
The MSPM0 devices go into a lower-power mode when executing the wait for event, _WFE( ), or wait for interrupt, _WFI( ), instruction. The low-power mode is determined by the current power policy settings. The device power policy is set by a driver library function. The following function call sets that power policy to Standby 0.
DL_SYSCTL_setPowerPolicySTANDBY0 ( );
STANDBY0 can be replaced with the operating mode of choice. For a full list of driverlib APIs that govern power policy, see this section of the MSPM0 SDK DriverLib API guide. Also, see the following code examples that demonstrate entering different operating modes. Similar examples are available for every MSPM0 device.