SLAAEH8 October 2024 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
In addition to the universal commands and the common-practice commands, manufacturers can implement device specific commands into devices. The following list shows some device specific commands that can be implemented.
Again, these commands can be implemented by device manufacturers but are not required. Device specific commands are not tested through the HART specification and are not implemented as tests in the HART test system.