SLAAEH8 October 2024 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
Figure 2-3 shows a simplified schematic of the V-to-I stage of the transmitter. This stage sets the current of the loop based on the voltage output of the DAC.
In this circuit, the DAC voltage is set across 100kΩ of equivalent resistance. The voltage at the opposite end of the 100kΩ is a virtual ground set by the feedback of the OPA333. The output of the OPA333 drives Q4 which sets the controls the loop current.
The current I1 flows through the 40.2kΩ resistor to set the LOOP– to a voltage below ground.
Current through the 40.2kΩ resistor is amplified 1000:1 with the 40.2Ω resistor and I2 is pulled from ground to LOOP–.