SLAAEI9 December 2023 MSPM0C1103 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1228
When you have finished downloading, the file content is shown in the SDK folder, which is "c:/ti/mspm0_sdk_xxx" by default, as shown in Figure 2-26, among which the mostly used folders are examples folder and docs folder.
Table 2-5 shows a summary of example coverage.
Supported by SDK | Platform | ||||
---|---|---|---|---|---|
IDE | CCS | Keil | IAR | ||
Compilers | TI Arm-Clang | GUN Arm | Arm/Keil Compiler | IAR Arm compiler | |
RTOS | FreeRTOS | ||||
Code examples | Driverlib/TI Dirvers(drivers) |
In nortos examples, you can also find three empty projects for users to build their own project.Table 2-6 shows the differences.
Example | Use Sysconfig | Include Library Files Into Project |
---|---|---|
empty | Yes | No |
empty_library | No | Yes |
empty_driverlib_src (Suggested) | Yes | Yes |
As for docs folder, the structure and the important documents are shown in Figure 2-27.