SLAAEN0 September 2024 MSPM0L1227 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
Tamper Event Detection allows the developer to configure one or more Tamper I/Os to trigger a timestamp to generate an interrupt to the CPU. The configured Tamper I/O needs to be an input to act as a tamper event trigger. To prevent false triggers, a digital filter circuit can detect whether the filter width is the same as configured. The input filter width can be selected from none, 30μs, 100μs, and 200μs.