SLAAEN0 September 2024 MSPM0L1227 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
Different peripherals have different signals and IOMUX mode allows the user to set the peripheral to a specific signal. Figure 2-6 shows the IOMUX mode is also the default mode for LFSS and is mainly useful when both VDD and VBAT are shorted or when LFSS is used as a secondary supply to operate on a secondary function at a different voltage level. One example of IOMUX mode is that using the device which is powered by 3V for the full analog performance and use LFSS act as a internal level shifter to operate serial-peripheral interface (SPI) connection to a CPU that requires 1.8V. Some limitations with IOMUX mode include the following: