SLAAEO5 September 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0L1105
In all regions of Flash memory in MSPM0, they will have a protection register known as CMDWEPROTx. They are dynamic registers that will unprotect sectors of memory according to which bit the user sets to zero. The memory remains unprotected until the user performs a flash operation. Upon performing any flash operation, the CMDWEPROTx register used automatically re-protects the memory by setting all bits back to one. Table 5-1 shows the protection registers used for all devices.
CMDWEPROTx Register | MSPM0L11XX / MSPM0L13XX | MSPM0G1X0X / MSPM0G3X0X | MSPM0C110X / MSPS003FX | MSPM0L122X / MSPM0L222X | All Future MSPM0 SOCs |
---|---|---|---|---|---|
CMDWEPROTA | x | x | x | x | |
CMDWEPROTB | x | x | x | x | |
CMDWEPROTNM | x | x | x | x | x |