SLAAEO5 September 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519 , MSPM0L1105
When creating the flashloader for any MSPM0 device, it is always vital that the flash algorithm performs modifications of each memory region separately. For example, if the user's application contains content for both the main and nonmain memory. Then the tool must take care of erasing and programming each memory region separately. This is to limit the exposure of the nonmain region as much as possible from other factors such as noise. Due to all the security configuration living within the region of nonmain memory, these cautions must be taken when attempting to modify it. For the ideal flow when programming, see Figure 5-1.