SLAU320AJ July 2010 – May 2021
This section describes the hardware connections to the JTAG interface of the MSP430 devices and the associated pin functions that are used during programming. This section also describes the software macro routines that are used to program a MSP430 target and the JTAG instructions that are used to communicate with and control the target through the JTAG interface.
The Replicator example project detailed in Section 3 implements the following high-level flow to clarify the minimum requirements for programming an MSP430 target memory.