SLAU367P October 2012 – April 2020 MSP430FR5041 , MSP430FR5043 , MSP430FR50431 , MSP430FR5847 , MSP430FR58471 , MSP430FR5848 , MSP430FR5849 , MSP430FR5857 , MSP430FR5858 , MSP430FR5859 , MSP430FR5867 , MSP430FR58671 , MSP430FR5868 , MSP430FR5869 , MSP430FR5870 , MSP430FR5872 , MSP430FR58721 , MSP430FR5887 , MSP430FR5888 , MSP430FR5889 , MSP430FR58891 , MSP430FR5922 , MSP430FR59221 , MSP430FR5947 , MSP430FR59471 , MSP430FR5948 , MSP430FR5949 , MSP430FR5957 , MSP430FR5958 , MSP430FR5959 , MSP430FR5962 , MSP430FR5964 , MSP430FR5967 , MSP430FR5968 , MSP430FR5969 , MSP430FR5969-SP , MSP430FR59691 , MSP430FR5970 , MSP430FR5972 , MSP430FR59721 , MSP430FR5986 , MSP430FR5987 , MSP430FR5988 , MSP430FR5989 , MSP430FR5989-EP , MSP430FR59891 , MSP430FR5992 , MSP430FR5994 , MSP430FR59941 , MSP430FR6005 , MSP430FR6007 , MSP430FR6035 , MSP430FR6037 , MSP430FR60371 , MSP430FR6041 , MSP430FR6043 , MSP430FR60431 , MSP430FR6045 , MSP430FR6047 , MSP430FR60471 , MSP430FR6820 , MSP430FR6822 , MSP430FR68221 , MSP430FR6870 , MSP430FR6872 , MSP430FR68721 , MSP430FR6877 , MSP430FR6879 , MSP430FR68791 , MSP430FR6887 , MSP430FR6888 , MSP430FR6889 , MSP430FR68891 , MSP430FR6920 , MSP430FR6922 , MSP430FR69221 , MSP430FR6927 , MSP430FR69271 , MSP430FR6928 , MSP430FR6970 , MSP430FR6972 , MSP430FR69721 , MSP430FR6977 , MSP430FR6979 , MSP430FR69791 , MSP430FR6987 , MSP430FR6988 , MSP430FR6989 , MSP430FR69891
How the LEA operates is briefly described in Section 17.2. It is not necessary to understand how the LEA works or the details of the LEA registers. The Digital Signal Processing (DSP) Library for MSP Microcontrollers offers easy-to-use APIs that use the functions of the LEA and provide a high-level environment to use the LEA in various applications. The DSP Library is a set of highly optimized API functions to perform many common signal processing operations on fixed-point numbers for MSP430 microcontrollers. The APIs automatically enable and use the LEA module if the LEA is available in the target device, and apply the optimal configurations to the LEA registers with the correct sequence. If the LEA is not available, the CPU is selected to perform the operations.
The full LEA commands are supported by the DSP Library APIs, which are listed in the DSP Library API Guide, Low-Energy Accelerator (LEA) Frequently Asked Questions (FAQ), and Benchmarking the Signal Processing Capabilities of the Low-Energy Accelerator on MSP430™ MCUs.
The following sequence of operations is an example of performing a vector-based algorithm using the LEA, DMA, ADC, and SPI.