SLAU367P October 2012 – April 2020 MSP430FR5041 , MSP430FR5043 , MSP430FR50431 , MSP430FR5847 , MSP430FR58471 , MSP430FR5848 , MSP430FR5849 , MSP430FR5857 , MSP430FR5858 , MSP430FR5859 , MSP430FR5867 , MSP430FR58671 , MSP430FR5868 , MSP430FR5869 , MSP430FR5870 , MSP430FR5872 , MSP430FR58721 , MSP430FR5887 , MSP430FR5888 , MSP430FR5889 , MSP430FR58891 , MSP430FR5922 , MSP430FR59221 , MSP430FR5947 , MSP430FR59471 , MSP430FR5948 , MSP430FR5949 , MSP430FR5957 , MSP430FR5958 , MSP430FR5959 , MSP430FR5962 , MSP430FR5964 , MSP430FR5967 , MSP430FR5968 , MSP430FR5969 , MSP430FR5969-SP , MSP430FR59691 , MSP430FR5970 , MSP430FR5972 , MSP430FR59721 , MSP430FR5986 , MSP430FR5987 , MSP430FR5988 , MSP430FR5989 , MSP430FR5989-EP , MSP430FR59891 , MSP430FR5992 , MSP430FR5994 , MSP430FR59941 , MSP430FR6005 , MSP430FR6007 , MSP430FR6035 , MSP430FR6037 , MSP430FR60371 , MSP430FR6041 , MSP430FR6043 , MSP430FR60431 , MSP430FR6045 , MSP430FR6047 , MSP430FR60471 , MSP430FR6820 , MSP430FR6822 , MSP430FR68221 , MSP430FR6870 , MSP430FR6872 , MSP430FR68721 , MSP430FR6877 , MSP430FR6879 , MSP430FR68791 , MSP430FR6887 , MSP430FR6888 , MSP430FR6889 , MSP430FR68891 , MSP430FR6920 , MSP430FR6922 , MSP430FR69221 , MSP430FR6927 , MSP430FR69271 , MSP430FR6928 , MSP430FR6970 , MSP430FR6972 , MSP430FR69721 , MSP430FR6977 , MSP430FR6979 , MSP430FR69791 , MSP430FR6987 , MSP430FR6988 , MSP430FR6989 , MSP430FR69891
The window comparator allows to monitor analog signals without any CPU interaction. It is enabled for the desired ADC12MEMx conversion with the ADC12WINC bit in the ADC12MCTLx register. In the following the window comparator interrupts are listed:
These interrupts are generated independently of the conversion mode selected by the user. The update of the window comparator interrupt flags happen after the ADC12IFGx.
The lower and higher threshold in the ADC12LO and ADC12HI registers have to be given in the correct data format. If the binary unsigned data format is selected by ADC12DF = 0, then the thresholds in the registers ADC12LO and ADC12HI must be written as binary unsigned values. If the signed binary (2s complement) data format is selected by ADC12DF = 1, then the thresholds in the registers ADC12LO and ADC12HI must be written as signed binary (2s complement). Altering the ADC12DF register or the ADC12RES register resets the threshold registers.
The interrupt flags are reset by the user software. The ADC12_B sets the interrupt flags each time a new conversion result is available in the ADC12MEMx register if applicable. Interrupt flags are not cleared by hardware. The user software resets the window comparator interrupt flags per the application needs.