SLAU834 October 2020 ISO7760 , ISO7762 , MSP432E401Y , TPS92520-Q1 , TPS92682-Q1
The SPI command box allows register read and write actions and it also records the SPI status sequentially. There are times when specific register settings may want to be controlled directly instead of through the simplified interface of the GUI. The following section is an example of doing reads and writes for when the LEDMCUEVM-132 is connected to the TPS92520EVM-133 to ensure proper communications.
To ensure a connection from the board to the TPS92520-Q1 exists, perform the following steps as shown in Figure 5-9.
The default value of 0x07 for the register 11 will be shown in the SPI Status window, see Figure 5-9.
To write data to the associated register address here is an example where channel 1 of the TPS92520EVM-133 is enabled using the write command: