SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
The peripheral region contains the memory-mapped peripherals on the three peripheral buses. The flash memory is also aliased in the peripheral region.
Type | Start | End | Description |
---|---|---|---|
Peripherals | 0x4000.0000 | 0x40FF.FFFF | Memory-mapped registers of peripherals on the peripheral buses |
Aliased flash memory | 0x4100.0000 | 0x41FF.FFFF | See Section 6.2.3.1 |