SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
The flash controller provides an erase verification mechanism to extend the lifetime of the flash bank. The CMDWEPROTx registers are used as an erase mask and are manipulated by the flash controller during the execution of the erase operation. At the end of all erase operations, the CMDWEPROTx registers are set to a fully protected state to prevent against inadvertent programming and must be re-configured before attempting another program or erase operation.