SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
The SPI module is located in power domain 1 (PD1) and as such is only active in RUN and SLEEP modes. If the SPI module is enabled by application software, an entry into STOP or STANDBY low-power mode forces the SPI module to be temporarily disabled while the device is in STOP or STANDBY mode.