SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
Configuration registers in SYSCTL can be locked out from writes to add a layer of robustness against unintended changes to the PMCU at runtime. To lock out the configuration registers from writes, set the ACTIVE bit in the WRITELOCK register in SYSCTL.
All SYSCTL registers are protected by the WRITELOCK functionality except for those listed below:
In addition to the overall SYSCTL configuration write lock feature, many SYSCTL registers also require a KEY value to be written in conjunction with the desire configuration data for the write to take effect.