SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
The GPAMP uses an input mux, N-MUX, to provide a selection of input channels for the inverting terminal of the amplifier. These inputs are configurable using the NSEL control bits. The non-inverting terminal of the amplifier is enabled using the PCHENABLE control bit and allows the input to be driven from the GPAMP_IN+ signal on a device pin.
A depiction of the input channel mapping is included in Table 13-18 below.
PCHENABLE | GPAMP Non-inverting Input | NSEL | GPAMP Inverting Input Channels |
---|---|---|---|
0x0 | Open | 0x0 | GPAMP output pad (GPAMP_OUT) |
0x1 | GPAMP_IN+ | 0x1 | GPAMP_IN- |
0x2 | GPAMP internal amplifier output | ||
0x3 | Open |