SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
The code region contains the flash memory used to store executable code and data. Accesses to the flash memory from the CPU through the code region are processed through the AHB bus matrix to the flash read interface directly. The flash memory is aliased to two address spaces in the code region: one returning ECC-corrected data, the other providing uncorrected (raw) data. See Section 6.2.3.1 for the detailed flash memory map.
The code region also contains the read-only memory (ROM) used for the TI device boot code and the bootstrap loader. The ROM is only available during the initial device boot process.