SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
DAC output can be connected to internal analog modules OPA, ADC & COMP or DAC_OUT pin by setting CTL1.OPS bit. Reset value of bits CTL1.OPS is 0. There are the following scenarios:
The CTL1.OPS bit must be set as 0 when pin DAC_OUT is configured as the input for ADC, OPA or COMP.