SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519
The OPA uses an input mux, M-MUX, connected to the programmable gain stage resistor ladder to allow the user to program the OPA for various analog signal chain configurations. These configurations include unity gain buffer, inverting/noninverting amplification, PGA, cascade amplification, and more.
A generalized depiction of the input channel mapping for M-MUX is included in Table 14-5 below. Please refer to the device-specific data sheet for a mode detailed depiction of the available M-MUX inputs.
MSEL | OPAx M-MUX Input Channels |
---|---|
0x0 | Open |
0x1 | OPAx_IN1- |
0x2 | GND |
0x3 | DAC_OUT |
0x4 | OPA[x-1]_RTOP |
The following sections provide examples of how P-MUX, N-MUX, and M-MUX can be configured for various amplifier modes.