SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
With the CTL1.REPEATTX bits the last character transmit will be repeated as defined by the register bits. A value of 0 in CTL1.REPEATTX bits will disable this mode and this function is only available in Controller mode. The transfer will be started with writing a data into the TX Buffer. Then the data will be repeatedly sent with the given value. The behavior is identical as if the data would be written into the TX Buffer that many times as defined by the value here. It can be used to clean a transfer or to pull a certain amount of data from a peripheral.
When REPEATTX is used it needs to be aligned with the data in the FIFO. So the below shown sequence should be used: