SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
The WWDT module provides one interrupt source which can be configured to source a CPU interrupt event. The WWDT interrupt conditions are given in Table 31-774.
Index (IIDX) | Name | Description |
---|---|---|
0 | INTTIM | Indicates that the WWDT interval timer period has expired |
The CPU interrupt event configuration is managed with the CPU_INT event management registers. See Section 8.2.5 for guidance on configuring the Event registers for CPU interrupts.