SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
The PLL startup time depends on the PLL feedback loop input frequency fLOOPIN and if the PLL is starting after previously running (for example, exiting a low-power mode) or starting for the first time after device boot. Table 2-6 lists the PLL startup times.
fLOOPIN | SYSPLL Startup Time (µs) | SYSPLL Startup Time on Exit From Low-Power Mode (µs) |
---|---|---|
32MHz ≤ FREQ | 5 | 3 |
16MHz ≤ FREQ < 32MHz | 15 | 12 |
8MHz ≤ FREQ < 16MHz | 25 | 20 |
4MHz ≤ FREQ < 8MHz | 40 | 35 |