SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
Period capture measures the period of a signal on an input CCP in TIMCLK cycles. On each positive (or negative) edge of the CCP input, the TIMx.CTR value is both captured into the TIMx.CC register to generate a capture event. The period capture time is equivalent to the difference between the starting value of the counter generated to the capture event, or time between reoccurring capture events for a periodic input signal.
Period Capture Configuration
Example using up-counting mode for rising-edge period capture
In up-counting mode starting from zero (CM = 2, CVAE = 2), TIMx channel 0 can be configured to generate a capture event from a rising edge input by setting CCOND = 1h. After enabling the counter, when a rising edge input is detected, the counter will capture the counter value in TIMx.CC. After the capture event, set the TIMx.LOAD value back to 0 to reset the timer counter for the periodic CCP input signal.
The expected internal timing for a period capture in up-counting mode using two rising edges is shown in Figure 27-14.