SLAU846B June 2023 – November 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507
The AESADV engine an efficient implementation of the Rijndael cipher (the AES algorithm) and a 128-bit polynomial multiplication (referred here to as ‘GHASH’, as per the AES-GCM specification). Rijndael is a block cipher with each data block consisting of 128-bits.
AES encryption requires a specific number of rounds depending on the key length. Supported key lengths are 128-bit, and 256 bit, requiring 10, and 14 rounds respectively.
The AESADV engine contains the AES ECB core and a dedicated 32-cycle polynomial multiplication module for performing GHASH operations (when GCM is configured). The polynomial multiplication operates in parallel with the AES core, if there is data available for both modules. This is the case after encryption of the first data block. While processing a data block, the next block can be pre-loaded immediately. When a block is pre-loaded, the first block must finish before additional data can be loaded.