The GUI status bar is located in the South
Pane shown in
Figure 4-22. The status bar
allows communication status to be monitored. The communication mode health indicator at
the bottom right is lit yellow when not connected, lit green when connected, or unlit
when in demo mode. When first opened, the GUI automatically attempts to connect with the
ULC1001-DRV2911 EVM via the USB2ANY interface. Upon successful connection, the green lit
connected indicator appears as in the bottom right corner of the status bar.
This connection takes approximately 25 seconds. Communication issues can include a
faulty USB2ANY interface connection, an incorrect target address, or an incomplete GUI
initialization. The
Read/Write Status Indicator on the bottom left of the status
bar cycles quickly through register names when the GUI is reading or writing registers
from the ULC1001-DRV2911 EVM. Double clicking the
Read/Write Status Indicator on
the status bar opens a floating window which displays the entire status log, shown in
Figure 4-23. Right-clicking this
floating window shows the options to clear log or save the log or set the size. The
status log is meant for recording Register Read/Write sequences. To create register
read/write scripts, see
Section 3.3.5.9.